AXIS#.MOTOR.R

Description

AXIS#.MOTOR.R sets the stator winding resistance phase-to-phase in ohms.


  • This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Range

0.001 to 650 Ω

Default Value

10 Ω

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.R 0x500B 0x18 UDINT 1000:1 - RW False
AXIS2.MOTOR.R 0x510B 0x18 UDINT 1000:1 - RW False